AXIS#.EIP.STREAMPERIOD
Description
This parameter allows modifying and configuring the interval at which the drive expects to receive position set-points from the fieldbus master when position streaming is configured and enabled (AXIS#.EIP.STREAMING = 1).
Example
-->AXIS1.EIP.STREAMPERIOD 500 -->AXIS1.EIP.STREAMPERIOD 500 [us]
Versions
Action | Version | Notes |
---|---|---|
Implemented | 02-11-00-001 |
General Information
Type |
Read/Write |
Units |
Microseconds |
Range |
500 to 10000 |
Default Value |
2000 |
Data Type |
|
Stored in Non-Volatile Memory |
Yes |
Variants Supported
EtherNet/IP drives: AKD2G-SPI
Fieldbus Information
Name |
ID |
Hex |
Data Type |
Access |
Units |
---|---|---|---|---|---|
AXIS1.EIP.QUICKSTOPACTION |
7554 |
1D82 |
Signed16 |
Read/Write |
- |
AXIS2.EIP.QUICKSTOPACTION |
73090 |
11D8 |
Signed16 |
Read/Write |
- |